2022-11-15 7:01 AM
2022-11-15 8:30 AM
Maybe you have done the measurements with oversampling ?
Or some other calculation error?
Or you just checked SFDR?
The ~ 12dB difference look suspicious... ;)
2022-11-15 8:39 AM
Oversampling is not involved (that also was done as an independent measurement with the expected results of slightly less that 4 bits improvement).
We used ENOB = (20log(FSR/StDev)-1.76)/6.02 where in this case FSR = 2^12 and StDev = 0.332 from 1024 samples collected using an LM4140 to generate a 1.25V input on the 0 channel. (The mean sample value was 1542.03 **** as expected)
2022-11-15 8:50 AM
I'd rather use RMS values, like full scale RMS input voltage compared to RMS noise over the used bandwidth.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.