2024-09-01 11:14 PM
Hi Sir ,
I need your help with some questions about SPWMI:
1. STM32Cube_FW_H7_V1.7.0 without Demo project, Could you provide a Demo project of SWPMI STM32H7?
2. As RM said,SWPMI can serve only as Master interface, Whether SWPMI can communicate with itself ? such as Board1 SWPMI (transfer) communicate with Board2 SWPMI (receiver) .
3.When internal transceiver is bypassed(SWP_TBYP=1),the SWPMI_TX、SWPMI_RX and SWPMI_SUSPEND signals can connect an external transceiver. I don't find the profile about external transceiver.Could you please prodive the specific device or profile of external transceiver?
Looking forward to your reply!
2024-09-04 6:19 PM
As I understand: SPWMI is just a master on STM32 MCU.
It does not have a slave receiver (or mode).
So, it cannot communicate with itself.
You might be able to test it with these single wire LED strips.
2024-09-05 12:31 AM
Thank you for your reply.
I have tested it and really cannot communicate with itself.
Now, I want bypass internal transceiver, and use SWPMI_TX、SWPMI_RX and SWPMI_SUSPEND signals connect an external transceiver, I don't find the device which satisfy ETSI TS 102 613 tcchnical in st.com .Could you please prodive the specific device(part number) of external transceiver?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.