2021-07-29 6:05 AM
Hi ST team,
I want to define a new section in the ld script so I can use that for variables that have to keep their values in case of soft resets.
I have made some changes in the script as follows,
.noinit (NOLOAD):
{
. = ALIGN(4);
_noinit = .;
*(.noinit .noinit.*)
. = ALIGN(4) ;
_end_noinit = .;
} >RAM
I have also defined a variable of this kind in the following way,
uint32_t tempVar __attribute__ ((section(".noinit"))) = 0;
At every soft reset, the value of this variable is preserved. However, at every hard reset, the variable is initialized with some garbage value.
What am I missing here?
Thank you.
Solved! Go to Solution.
2021-07-30 5:51 AM
You can look at the RCC->CSR register to determine the source of the reset and handle them differently, if you want.
2021-07-29 6:21 AM
>>What am I missing here?
Ordering, what startup.s is actually doing, and the scope of the beginning/ending symbols in reality.
Watch also for where stack falls, or other code running, ie loader or system loader.
Content will be random at power-up.
2021-07-29 6:44 AM
What does a soft reset vs hard reset mean here? RAM won't be preserved on a power cycle.
2021-07-29 10:36 PM
Hi Tesla DeLorean,
"Content will be random at power-up."
So, the content of that variable will be garbage at power-up, right?
Is there any way to prevent that from happening? Can we initialize it on power-up or something?
2021-07-29 10:38 PM
Hi TDK,
What I mean by hard reset is the power cycle of the MCU. And by soft reset, I mean that giving reset pulse on the MCU using the reset switch.
2021-07-30 5:50 AM
2021-07-30 5:51 AM
You can look at the RCC->CSR register to determine the source of the reset and handle them differently, if you want.
2021-08-02 5:49 AM
Is it possible to initialize a variable on the power cycle, but preserve it on soft resets in RAM memory only?
Is there any other way than NOLOAD?
And regarding the RCC->CSR register;
We are using STM32l562CEU6. So in our case, there is no POR-related flag. But there is a BORRST flag. And default value of the VDD cut-off for BOR is 1.71V.
I kept a check of the previous reset condition using the RCC_FLAG_SFTRST and RCC_FLAG_BORRST with __HAL_RCC_GET_FLAG(__FLAG__) API. But If I give a pulse on the NRST pin of the MCU or power cycle the MCU, I can not differentiate using the flag check.
Am I missing something here?
2021-08-02 6:00 AM
>>Is it possible to initialize a variable on the power cycle, but preserve it on soft resets in RAM memory only? Is there any other way than NOLOAD?
Not via magic. NOLOAD means that the linker/startup code leave it alone..
You could use a signature and check over the content to determine if you want to keep the data or memset() it to zero.
What's the end-goal/purpose you're trying to achieve here? Any NV/BKP RAM in this part? Battery backup for RTC/BKP in design?
2021-08-02 6:46 AM
What we want here is that a variable should be initialized with a specific value at every power cycle. At run time the value of the variable will be updated. But at every soft reset( i.e; pulse on NRST pin of the MCU), it should be preserved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.