2017-05-28 2:25 AM
Dear All friends,
I am a new developer to code the encoder interface of STM32F301 TIM2, based on STM32CubeMX. the code generated by STM32CubeMx does not work. I followed the instruction of TIM2 encoder mode. Please see the code below,
void SystemClock_Config(void);int16_t counter;int main(void){/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init(); /* Configure the system clock */ SystemClock_Config();/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_TIM1_Init(); MX_TIM2_Init(); MX_TIM16_Init(); MX_TIM17_Init(); MX_USART1_UART_Init();HAL_TIM_Encoder_Start_IT(&htim2,TIM_CHANNEL_1 + TIM_CHANNEL_2);
TIM2->CNT = 0; while (1) { int16_t count1; count1 = TIM2->CNT & 0x0000ffff; }}
I got some problems,
1. After complied, got error message 'Warning[Pe550]: variable 'count1' was set but never used'. I saw some samples code use TIM2->CNT to read the number of encoder. but in my application, got the compiler warning and the variable is not available.
2. the interrupt of the code is working. How to read the counter of encoder?
3. There is no sample code for TIMER encoder mode that is generated by STM32CubeMX. Do any experts have any sample code with STM32CubeMX?
Thanks in advance!
Jiannong
#stm32f3-timer-encoder-mode2017-05-29 2:11 AM
Hi
Jiannong.Zhou
,Please make sure that you configure the GPIO settings correctly and
provide your
Timer
configuration for more check.
The STM32CubeF3 does not contains an encoder example.
But,
you can inspire from anotherexample with STM32Cube package to develop your application, like STM32CubeF4 which has the 'TIM_Encoder' example
available at this path:
STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_Encoder
Imen
2017-05-29 6:56 AM
Hi Imen,
thank you very much for your comment and suggestion. I will try it out.
regards,
Jiannong
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.