2019-04-17 11:23 AM
Hi guys, I am trying software timers without using interrupt
SysTick->CTRL = 0x5;
SysTick->LOAD = 0xFFFFFF;
SysTick->VAL = 0;
when start the program, what will happen with SysTick->VAL = 0;
it is value start with 0xFFFFFF or 0?
2019-04-17 11:29 AM
Can you not simply observe and see experimentally?
The SysTick is a 24-bit DOWN COUNT, it typically loads the value specified, and when it gets to zero it interrupts and reloads.
2019-04-17 11:48 AM
Unfortunately I dont have my MCU now, I am at another city for now, but I got the point in datasheet thank you
2019-04-17 11:49 AM
Better study the RTC then.
Try to use interrupts with timers.
Interrupts is something important to learn.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.