2009-03-18 11:35 PM
System Memory Boot Mode and TIM1 usage
2011-05-17 3:18 AM
no and no.
but you can make your own bootloader and keep it protected in a section of flash. too bad ST won't release the source of their bootloader, it'd make things easier for you. they do provide DFU code to flash via USB (but if your code must be secure, I wouldn't use it; it might have security issues in the form of exploitable bugs).2011-05-17 3:18 AM
Hello,
we are testing the boot loader feature at the moment. For your interesst: 1. it is possible to jump into the boot loader from your application. So you do not need to modify the BOOT0/BOOT1 pins. 2. the boot loader does not modify the remap-bit for USART1. So you can remap the USART1 to other pins. At the moment we do not know if the autobaud feature of the bootloader is hard coded against the standard USART pins. We will test it this week. Maybe it is flexible at this point, so you can use the boot loader feature even together with TIM1!!! Regards Wolfgang Beck2011-05-17 3:18 AM
Hi,
You are right. We finally failed to use the remapped USART1 for the boot loader. Has anyone there implent his own boot loader? Regards Wolfgang Beck2011-05-17 3:18 AM
Quote:
1. it is possible to jump into the boot loader from your application. So you do not need to modify the BOOT0/BOOT1 pins. Wolfgang Beck It's possible with a jump to 0x1FFF F000? Are there configurations before jump? jerome [ This message was edited by: j.vaquie on 19-03-2009 12:05 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.