2014-06-28 2:52 AM
hello
I want to use synchronous mode Usart. but i dont know how to set clock pin to for example 10 MHZ. please help me. thanks #stm32 #synchronous #usart2014-06-28 5:29 AM
10 MHz might be a challenge. You'd get there by setting the baud rate, and enabling the synchronous clocking mode.
You'd probably need to use OVER8 mode, and run the CPU/BUS at a multiple of 80 MHz STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\USART\Synchronous2014-06-28 8:08 AM
10 MHz might be a challenge. You'd get there by setting the baud rate, and enabling the synchronous clocking mode.
You'd probably need to use OVER8 mode, and run the CPU/BUS at a multiple of 80 MHz STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\USART\SynchronousThanks for your Quick answer.
I need 10 MHZ clock, because i want to communicate with a ccd sensor that its clock works in 10 MHZ. The clock of the USART2 (PCLK1) is 36 MHZ . Is it possible that i set PCLK1 to 10MHZ ?2014-06-29 7:27 AM
Are you sure the data format/framing are compatible? Wouldn't SPI (Slave clocked at 10 MHz) perhaps be a better choice?
Other STM32 family members have a DCMI interface for camera type applications.2014-07-05 11:11 PM
''Are you sure the data format/framing are compatible? Wouldn't SPI (Slave clocked at 10 MHz) perhaps be a better choice?
Other STM32 family members have a DCMI interface for camera type applications.'' Yes I'm sure, because that data comes from the sensor is in usart protocol that have 10 bits , 8 bits data with 1 stop bit and 1 start bit. i think spi cant help me because its frame has 8 bits . BUT i set PCLK1(Clock of APB1) to 9MHZ with prescalers but PA4 pin (USART2_CK) was not 9MHZ in oscilloscope? why? i changed a line in system_stm32f10x.c static void SetSysClockTo72(void) { __IO uint32_t StartUpCounter = 0, HSEStatus = 0; /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration ---------------------------*/ /* Enable HSE */ RCC->CR |= ((uint32_t)RCC_CR_HSEON); /* Wait till HSE is ready and if Time out is reached exit */ do { HSEStatus = RCC->CR & RCC_CR_HSERDY; StartUpCounter++; } while((HSEStatus == 0) && (StartUpCounter != HSEStartUp_TimeOut)); if ((RCC->CR & RCC_CR_HSERDY) != RESET) { HSEStatus = (uint32_t)0x01; } else { HSEStatus = (uint32_t)0x00; } if (HSEStatus == (uint32_t)0x01) { /* Enable Prefetch Buffer */ FLASH->ACR |= FLASH_ACR_PRFTBE; /* Flash 2 wait state */ FLASH->ACR &= (uint32_t)((uint32_t)~FLASH_ACR_LATENCY); FLASH->ACR |= (uint32_t)FLASH_ACR_LATENCY_2; /* HCLK = SYSCLK */ RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1; /* PCLK2 = HCLK */ RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE2_DIV1; /* PCLK1 = HCLK */RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV8; //72MHZ/8 = 9MHZ
. . . }2014-07-06 4:52 AM
So what clock DO you see? And how have you configured the USART?
I'd guess 4.5 MHz, why run APB1 at 9 MHz, wouldn't a higher multiple work better? Review the USART block diagram in the manual, and the GTPR register.2014-07-07 12:22 AM
The usart2_ck pin was about 2.4 MHZ in oscilloscope. I need 10 MHZ
clock to joint to my sensor clock and 9 MHZ APB1 clock is reachable by prescalers.but i found maybe usart clock pin does not correspond to APB1 clock. Am i right? so 10 MHZ for usart clock pin is unreachable?!!? Its my configuration code : GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO ,ENABLE); RCC_APB1PeriphClockCmd( RCC_APB1Periph_USART2 , ENABLE ); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;//GPIO_Mode_IPU; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitTypeDef USART_InitStructure; USART_ClockInitTypeDef USART_ClkInitStructure; USART_InitStructure.USART_BaudRate =BaudRate ; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_ITConfig(USART2,USART_IT_RXNE,ENABLE); __nop(); __nop(); USART_ClkInitStructure.USART_Clock=USART_Clock_Enable; USART_ClkInitStructure.USART_CPOL=USART_CPOL_Low; USART_ClkInitStructure.USART_CPHA=USART_CPHA_2Edge; USART_ClkInitStructure.USART_LastBit=USART_LastBit_Enable; USART_ClockInit(USART2, &USART_ClkInitStructure); USART_Cmd(USART2, ENABLE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.