2015-05-07 10:07 PM
Hi,
The STM32F4 on my application uses an 8MHz crystal, and synthesized to run at a bus speed of 168MHz. I'm doing some signal processing that really only requires a speed of 168MHz after a signal is detected. The detection of the signal could be accomplished with a clock speed as low as the crystal itself (8MHz) Can someone please advise me on the steps on how to do this dynamically - if for example it's running at 168MHz, what should be done with peripherals, etc, to safely set the operation to a lower frequency, and upon a certain event, reset the clock speed higher. Appreciate any links, suggestions or steps (checked through this site but found nothing) Thanks! #stm32f4 #clock-speed2015-05-08 1:40 AM
At 168 MHz you're running off the PLL.
To switch to a lower speed, you will need to first switch from the PLL to another oscillator i.e. HSI or HSE. If that's your target oscillator, you then just need to update the Flash latency and bus dividers as appropriate.Most likely though you want to run the PLL at a different frequency so you need to:Then turn off the PLL.Then change the PLL dividers and multipliers.Then turn the PLL back on.While waiting for lock you can update the bus dividers for your new frequency, as well as e.g. UART baud-rate dividers.The switch to PLL.Caveats:Anything asynchronous (e.g. RS232) cannot maintain baud rate over the switchover - it's bound to glitch. I'm fortunate in having RTS/CTS handshaking so I can stop a remote device from sending me stuff.I think there might also be issues with DMA when some bus-division-ratios change (see errata) so I like to suspend e.g. SDIO transfers as well.While you're on HSI/HSE you can't service e.g. USB.Hope this helps,Danish2015-05-08 10:28 AM
it's bound to glitch.
Indeed, it's very hard to switch things. It's not sufficiently atomic, and stuff will glitch.Changing baud rates you want to confirm TC is done otherwise stuff changes mid byte.If it's a power play, consider if you can run at high speeds and have the idle loop WFI, reduce the period of ticker interrupts, etc.2015-05-08 11:58 AM
2015-05-08 12:05 PM
DA,
Your suggestions are appreciated and give me enough information to investigate the manual and try tackling it. The nice thing is, I have really one operation to suspend - the Timer interrupt - that is used to check (detect) for a signal (through the ADC) at a prescribed rate. The rest of the peripherals (such as USB, SPI memory writes and RS232) won't get executed until (after) that event occurs, where I would have to stop just timer 6 and change speed, then restart the needed interfaces.2015-05-08 12:45 PM
One of the easier routes might be to drop the APB clocks to some minimum you need for baud rate, timers, etc.
Then increase/decrease the CPU clocking, and adjust the APB so they remain consistent.2015-05-08 4:52 PM
also sounds like a plan to try, thanks!
I've seen various documents on power consumption, but none that really spelled out specifics with respect to clock and/or bus speed. In your experience, and given the suggestion you (and DA) provided, what kind of power saving (range) could be expected ? I would think there's no direct proportional relationship between clock speed and power consumption...or is that a bad assumption?2015-05-08 8:30 PM
Well tight loops with while(1); can be real killers.
It's usually all the things you have attached/interfaced to the system that pull the most power. So you really have to measure and think about things at a system level, than worry about the uA/MHz quoted in the data sheets. CMOS gates draw current when there states change, so most current is seen as it clocks, and the more rapidly it clocks, the more things change.2015-05-08 9:41 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.