2021-07-08 2:40 AM
Hi, I can not connect to my STM32F767ZIT on custom PCB.
It is frustrating as everything seems to be fine:
I was trying to use ST-LINK and Cube Programmer, they work with another board so the problem is not with these programs or with drivers. I was also trying to use multiple ST-LINKs, but I had the same result with all of them.
It seems that the problem is with board or maybe I used wrong settings in ST-LINK utility? I was trying multiple modes, frequencies and reset modes, also I used default settings which should be fine?:
Thank you for any advice!
2021-07-08 2:59 AM
check if you did not disable SWD or you did not sleep MCU, try flash with BOOT0=HIGH
2021-07-08 7:47 AM
It's more likely to be a hardware issue than incorrect settings in STM32CubeProgrammer. Check for correct connections, solder bridges. Show the schematic if you can.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.