2021-10-06 11:50 PM
Hello,
I wanted to know some suggestion regarding a project, and adding FOTA support in it.
The project is stm32f405 based and it configures the gsm module as a server and one can make request and get response using https request.
I wanted to update the firmware of the stm32f405 using the gsm module, I have looked into muc like the STM32WB series that have FOTA implemented for Bluetooth, and some basic principle used by the implementation. But I wanted to use the existing stm32f4 mcu and don't want to port my project to stm32wb.
Any suggestion(hardware or sotfware) on how can I implement the FOTA.
Thankyou.
Solved! Go to Solution.
2021-10-07 1:36 AM
On the STM32 side look at the IAP (In App Programming) example. Look also at support for using HTTP/GET or FTP as a means of pulling data from servers.
2021-10-07 1:36 AM
On the STM32 side look at the IAP (In App Programming) example. Look also at support for using HTTP/GET or FTP as a means of pulling data from servers.
2021-10-07 1:39 AM
Thank you, I will look into it.
2021-10-07 5:01 AM
What are your though of OpenBLT. Should I use OpenBLT as a starting point and modify it to work with the gsm module or should I use the IAP driver as starting point?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.