2016-02-22 5:02 PM
Hello,
I am currently developing a custom STM32 programmer using the STVP programming toolkit. For my application two STM32 chips are connected to a single computer via two separate ST-LINK's. Looking at the STVP documentation, I can't seem to figure out how to select between the two ST-LINK's. I see that I can specify the port but that seems to just be USB, is there a way to select the ST-LINK by serial number or COM port?Thanks,Alex #stvp-st-link-developer2016-02-23 1:59 AM
Hello,
No, you can't choose a serial number to select the STLink with the programming toolkit. You can use the example installed in STVP directory (STVP_CmdLine.exe), you can choose the STlink id with ''Tool_ID'' arg: [-Tool_ID=x] ==> ST-LINK Programming Tool ID (0, 1, 2...) It is not very convenient because you have to try to know which STLink is ID 0 and 1. If the devices connected to the STLink are the same and you want to program the same application program, you can use the ''NbTools'' arg instead: [-NbTools=x] ==> Number of ST-LINK Tools with same device connected (Tool_ID is automatically incremented) If you want to use the STlink's Serial Number, you can use the STLink Utility (that has also a command line tool).Rgds,
LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.