2013-01-20 6:53 AM
Hi,
It does not matter if i config usart or not,when i open hyperterminal,and execute my program,i am getting junk on the screen ,like this : þÿÿÿÿÿøÿþÿÿÿÿÿÿÿþÿÿüÿÿÿÿÿÿÿúÿÿÿÿÿòþÿÿÿÿÿÿÿÿÿÿþÿÿÿþÿÿþÿþþÿÿøþÿÿÿÿÿÿÿÿþøÿÿðÿÿÿÿÿÿöÿÿþÿÿþÿþÿÿÿÿÿÿÿÿÿÿÿÿþÿÿÿÿÿÿöÿÿÿÿþÿÿÿøÿÿÿÿÿþÿÿÿÿþÿÿÿÿÿöÿþÿÿÿÿöþÿþ÷ÿÿÿñþÿðÿìÿÿÿÿüÿÿÿÿÿÿÿÿüÿþÿÿòÿÿÿÿÿÿÿÿöþÿÿþþÿÿþ What maybe the problem? i am also using sd card interface ,maybe there are some grounding issues ? Thanks Michael2013-01-20 7:19 AM
Stick a scope on the pin and see if the signal occurs when you're accessing the SD card or other interfaces. If you can figure out the nature of the signal and when it occurs you'll be able to bisect the issue and debug it.
More likely a short, or a conduction path via a resistor or chip pin.2013-01-21 1:41 AM
Hi Clive,
its the stm3240g-eval board,in the board manual it says : A 1 Gbyte or more MicroSD Card connected to the STM32F407IGH6 SDIO is available on the board. MicroSD Card detection is managed by the standard I/O port PH13. The MicroSD Card shares I/Os with motor control, RS-232 and audio meaning that the sd card and the usart shar the I/O,is there anyway that i can use simultaniosaly the usart and the microSD? Thanks2013-01-21 5:19 AM
''the SD card and the usart share the I/O, is there anyway that i can use simultaniosaly the usart and the microSD?''
I find this the fundamental problem with ''DevKits'' that come loaded with loads of peripherals!
You'll just have to look at the board schematics and see what you can figure out...
It might be easier to use a Discovery board instead...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.