2010-06-29 3:01 PM
Strange situation for a newbie
2011-05-17 4:56 AM
I believe it is simple. PA15 default after reset is JTAG Data In. Use another pin.
Cheers, Hal2011-05-17 4:56 AM
I have thought about that and I used this:
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable | GPIO_Remap_SWJ_NoJTRST, ENABLE); since I am using SWJ 3pin, shouldn't this be OK to release that pin? This is my GPIO config: void Port_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable | GPIO_Remap_SWJ_NoJTRST, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_GPIOB|RCC_APB2Periph_GPIOC|RCC_APB2Periph_GPIOD|RCC_APB2Periph_AFIO, ENABLE); // SPI Bitbang ----------------------------------------------------------------- GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); // SST25 CS------------------------------------------------------------------------ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); } Thanks Frank2011-05-17 4:56 AM
Hi,
The remap is part of the AFIO IP, so you are using the IP before enabling its clock: RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_GPIOB|RCC_APB2Periph_GPIOC|RCC_APB2Periph_GPIOD|RCC_APB2Periph_AFIO, ENABLE); //then you can call GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable | GPIO_Remap_SWJ_NoJTRST, ENABLE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.