2014-09-22 4:55 PM
Hi All
Cube 4.3.1/Keil/F4:When generating a cube project that includes a USB(HS) mass storage driver, if the file ''USBD_Storage_if.c'' already exists in your project AND has been modified within *USER CODE BEGIN* for the hooks, when you re-generate the project, the ''STORAGE_IsReady_HS()'' function ends up as the following:int8_t STORAGE_IsReady_HS (uint8_t lun){ /* USER CODE BEGIN 11 */ /* USB Mass storage Standard Inquiry Data */int8_t STORAGE_Inquirydata_HS[] = {//36 /* LUN 0 */ 0x00, 0x80, 0x02, 0x02, (STANDARD_INQUIRY_DATA_LEN - 5), 0x00, 0x00, 0x00, 'S', 'T', 'M', ' ', ' ', ' ', ' ', ' ', /* Manufacturer : 8 bytes */ 'P', 'r', 'o', 'd', 'u', 'c', 't', ' ', /* Product : 16 Bytes */ ' ', ' ', ' ', ' ', ' ', ' ', ' ', ' ', '0', '.', '0' ,'1', /* Version : 4 Bytes */}; /* USER CODE END 11 */ }If this file is manually deleted before re-creating the cube project - it is created OK.Any ideas?2014-10-08 1:21 AM
Hi JasonP,
Thank you for bringing this issue to our attention. We’ll pass it along to our STM32CubeMX team. Keep an eye out for the next update!Regards,Heisenberg.2014-11-07 2:41 AM
Dear user,
we do not reproduce your issue. Thanks in advance for providing us with your ioc file and the code that was added to the user section. Note, user section tags should not be modified (in your extract we should see section 1 and not section 11). Best regards2014-11-09 3:20 PM
Hi
Updating to cubeMX 4.4 seems to have fixed this issue.Thx.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.