2017-07-11 7:12 AM
I am using multiple AD7793 ADCs across 2 SPI buses. I have written the software for this for an STM32F205 using the STMCube construct.
I can communicated with the ADCs on either bus but when I try to talk to both buses SPI3 becomes unresponsive, not providing operation compete callbacks.
I am using the HAL commands:
HAL_SPI_TransmitReceive_IT - for recovering data, sending read commands and reading back chars
HAL_SPI_Transmit_IT - for sending commands
I am using the following callbacks:
HAL_SPI_TxRxCpltCallback - Read complete
HAL_SPI_TxCpltCallback - Command complete
I am using SPI2 and SPI3 and they are both setup the same (via STMCube generated code).
Is there a limitation of using 2 SPI ports at the same time?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.