2014-03-16 2:54 PM
Dear all,
after some issues using a programmer as parport interface, i am trying to program stm32f405 with a cheap stlink-V2, but still without success. I attach the openocd log, maybe someone can help me. Open On-Chip Debugger 0.8.0-dev-00381-gf91390f (2014-03-14-22:58) Licensed under GNU GPL v2 For bug reports, read http://openocd.sourceforge.net/doc/doxygen/bugs.html Info : This adapter doesn't support configurable speed Info : STLINK v2 JTAG v17 API v2 SWIM v4 VID 0x0483 PID 0x3748 Info : using stlink api v2 Info : Target voltage: 3.208404 Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints target state: halted target halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08001a20 msp: 0x20020000 Info : accepting 'telnet' connection from 4444 ██ telnet localhost 4444 Trying ::1... Trying 127.0.0.1... Connected to localhost. Escape character is '^]'. Open On-Chip Debugger > flash probe 0 device id = 0x10016413 flash size = 1024kbytes device id = 0x10016413 flash size = 1024kbytes flash 'stm32f2x' found at 0x08000000 > flash write_bank 0 bin/gasc.bin 0 jtag status contains invalid mode value - communication failure error waiting for target flash write algorithm error writing to flash at address 0x08000000 at offset 0x00000000 in procedure 'flash' jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 100ms jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 300ms jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 700ms jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 1500ms jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 3100ms jtag status contains invalid mode value - communication failure Polling target stm32f4x.cpu failed, GDB will be halted. Polling again in 6300m May be the fact i didn't connected NJTRST pin to the programmer (should'n be mandatory) ? Every help si appreciated. many thanks angelo2014-03-16 3:23 PM
What if you use the Windows ST-LINK utilities?
Connect in SWD mode?2014-03-27 6:43 AM
For support you may get help quicker if you post to the OpenOCD mailing list.
As a guess I would say that you are not erasing the flash first. Depending on what your are trying todo a better cmd may be to use write_image. flash write_image erase stm32f4x.bin 0 Also use the generated elf rather than generating a binary. Newer versions of OpenOCD have a programming helper script - see http://openocd.sourceforge.net/doc/html/Flash-Programming.html#Flash-Programming SpenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.