2025-02-19 12:59 AM
Hello,
Does the STM32U575CG/I (48-pin package) support USB communication, or is USB functionality only available on higher pin-count variants?
Thank you.
2025-02-19 1:05 AM
Hi @joaorego
All packages for this family support USB!
575 = STM32U575xx with OTG
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-19 1:17 AM
But what about the USB supply voltage? Will it be sourced directly from VDD? Can I still supply VDD with a voltage lower than 3V?
2025-02-19 1:23 AM
USB requires 3.3 V power.
2025-02-19 1:40 AM
Hi @joaorego
As explained in the footnote of Table 150. OTG_FS characteristics (continued) in page 304,
USB functionality is ensured down to 2.7V, but some USB electrical characteristics are degraded in 2.7 to 3.0 V range.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.