2024-04-08 7:23 PM
The example project I'm basing most of my code off of is from the STM32CubeU5 MCU package v1.4.0 (Projects\STM32U575I-EV\Applications\FileX\Fx_uSD_File_Edit). I'm looking to eventually apply this code to my primary project that saves JPEGs from a camera into the SD card. The plan is that each time a certain amount of JPEG data arrives (currently using an amount of 38,400 bytes), I call fx_file_write() to write the data into a file on the SD card. But the writes do not seem to be fast enough for my application (the 38KB of data arrives every 10ms, but each file open/write/close is taking between 30-60ms; I'm using LED toggles to determine these timing measurements). I'm opening this post to ask about ways to speed up the FileX write calls.
2024-04-08 7:26 PM - edited 2024-04-08 7:27 PM
(OP replying here) One thing I've considered is that the SD card itself does not support fast enough writes. But I've checked it and believe it should not be an issue (please correct me if I'm wrong).
Here are my SD card's features:
2024-04-15 1:47 AM
Hi. Just checking to see if anyone has any updates about this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.