2022-10-25 3:05 AM
Dear Sir.
I need the output of the ADC to be signed .
the adc is configured .
/** Common adc1 configuration */
hadc->Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc->Init.Resolution = ADC_RESOLUTION_14B;
hadc->Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc->Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc->Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc->Init.ExternalTrigConv = ADC_EXTERNALTRIG_LPTIM2_CH1;
hadc->Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISINGFALLING;
hadc->Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc->Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc->Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc->Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hadc->Init.LowPowerAutoWait = DISABLE;
hadc->Init.ContinuousConvMode = DISABLE;
hadc->Init.DMAContinuousRequests = ENABLE;
hadc->Init.OversamplingMode = DISABLE;
hadc->Init.DiscontinuousConvMode = DISABLE;
hadc->Init.NbrOfConversion = ADC_CHANNELS;
hadc->Init.GainCompensation = 0;
if (HAL_ADC_Init(hadc) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_15;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_391CYCLES_5;
sConfig.SingleDiff = ADC_DIFFERENTIAL_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 8192;
sConfig.OffsetSign = ADC_OFFSET_SIGN_NEGATIVE;
if (HAL_ADC_ConfigChannel(hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
the adc output register is drfined as
__IO int aADCxConvertedData[ADC_CONVERTED_DATA_BUFFER_SIZE * ADC_CHANNELS];
Any idea why I don get the aADCxConvertedData negative ?
Please Advise.
2022-11-30 1:55 PM
Hi @Community member,
ADC_OUTPUT = Full_scale x Vinput/VREF+
Vinput that is the channel input is always between Vref+ and Vref- (for Nucleo-U5 Vref+=VDD and Verf-=VSS). As Vinput is always positive, the ADC_OUTPUT (converted data) is always positive.
Real value should be got according to your sensor documentation, which is function of Vinput or ADC_OUTPUT values. This real value can be negative or positive.
BR,
Younes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.