2024-06-21 1:51 AM
Hi,
I'm currently using the STM32U575 to develop a product, and my clock configuration is set to the maximum of 160MHz because I'm dealing with a large amount of data. I have two SPI channels collecting data at a sampling rate of 20kHz, with each sampling returning 70 data points. During operation, I encounter Hardfaults on the bus, with bus fault information showing IBUSERR or PRECISERR. I suspect that the CPU and DMA are competing for the bus, causing errors. However, I found that by adjusting the wait state parameter in the RAMCFG configuration to 1 or 2, the system runs much more stably. Is RAM access unstable at 160MHz? Do you have any experience with configuring RAM wait states, or how to ensure reliable operation?
2024-06-22 11:23 AM
Dear @OneLine ,
you can refer to slide 8 here
if your configuration case is not inline , it is not normal and we never had such issue , you may check the race conditions from different masters writing on same memory . If possible to know if particular addresses are impacted ? To identify which RAM .
hope it helps ,
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.