2017-04-25 10:14 PM
Hello,
I am working with the STM32L476G-Discovery board. I am testing the examples applications and I have found an error in the demonstration application regarding to the soundmeter feature.* With the *.bin file provided in the Binary folder the application works normally. I mean, that you can see in the Display how it changes the sound intensity in dB when it is louder or not.* but, with the IAR source code project, when you program the demonstration application in the STM32L476G-Discovery board, the soundmeter feature doesn't function anymore, it shows a constant value of 120dB in the Display of the board.
I think again, somebody change something in the code and he forgot to test it. Typical, very typical.Please, check this error as soon as possible and provide a change in the software to solve this problem.Regards,Daniel
Solved! Go to Solution.
2017-05-09 9:04 AM
Hi
Martinez.Daniel
I already tested successfully the Demo with the same board andI'm not able to reproduce your issue !
The program worked great and I can
see the sound
in dB changed in the Displa
y, I'm using:STM32L476G-DISCO board (MB1184C)
IAR version 7.70
STM32Cube_FW_L4_V1.7.0
I'm interested to knownif there is a difference with your use case compared to the one I'm testing.
So, could you please precise which IAR and firmware package are you using ?
Thanks
Imen
2017-04-25 10:40 PM
I think again, somebody change something in the code ...
Not necessarily.
Beside of different startup code and memory layout, varying project settings, like optimization level, can cause such issues - if the code itself is not safe for optimization.
... and he forgot to test it. Typical, very typical.
Fully agree with that.
2017-04-26 1:21 AM
Beside of different startup code and memory layout, varying project settings, like optimization level, can cause such issues
+1
Doubly so, as the core of the audio demo code is provided as an IAR-only binary blob ([STM32Cube_FW_L4_V1.5.0]\Projects\STM32L476G-Discovery\Demonstrations\Modules\soundmeter\lib_smr_CM4F_IAR.a).
Release Notes wrote:
Restriction: SoundMeter and GuitarTuner applications not available pending audio libraries availability for Keil.
readme.txt wrote:
- Binary file generated with IAR Workbench V7.40 in High optimization modeMaybe works as eye catcher, but very useful as an example, if you ask me.
JW
2017-04-26 4:11 AM
For me, the perceived quality of the Cube examples 'rubs off' at the Cube package in general. (Or vice versa).
Sometimes, less is more ...
2017-05-08 10:37 AM
Not much interest from the people of ST on this subject :(
2017-05-09 9:04 AM
Hi
Martinez.Daniel
I already tested successfully the Demo with the same board andI'm not able to reproduce your issue !
The program worked great and I can
see the sound
in dB changed in the Displa
y, I'm using:STM32L476G-DISCO board (MB1184C)
IAR version 7.70
STM32Cube_FW_L4_V1.7.0
I'm interested to knownif there is a difference with your use case compared to the one I'm testing.
So, could you please precise which IAR and firmware package are you using ?
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.