2016-10-27 1:58 AM
Hello,
I made a simple project with usb host msc on STM32L476G-DISCO ,
The application works after reset, the usb stick is correctly enumerated.
After Disconnect and Reconnect of the USB-stick ,the Enumeration of the stick hangs.
I put some more debug information in usbh_core.c and usbh_ctrlreq.c
to show some states.
I made an identical project with nucleo-f429 and it works without problems with this usb stick.
debug output:
Hi test start
CLOCK CONFIGURATION
HCLK : 80000000
PCLK1 : 80000000
PCLK2 : 80000000
SYSCLK : 80000000
HSE -> PLL -> SYSCLOCK
000450 USBH_Process gState: 0
000960 USBH_Process gState: 2
000960 USB Device Attached
001460 USBH_Process gState: 5
001460 EnumState : 0
001460 USBH_CtlReq RequestState: 1
001460 USBH_CtlReq RequestState: 2
001460 USBH_HandleControl Control.state : 1
001460 USBH_HandleControl Control.state : 2
001460 USBH_HandleControl Control.state : 3
001460 USBH_HandleControl Control.state : 4
001461 USBH_HandleControl Control.state : 9
001461 USBH_HandleControl Control.state : 10
001461 USBH_Get_DevDesc ok.
001461 EnumState : 1
....
....
001979 MSC Device ready
001980 MSC Device capacity : 3516923392 Bytes
001980 Block number : 15257599
001980 Block Size : 512
080223 USB Device disconnected
080223 USBH_Process gState: 3
080223 USBH_Process gState: 0
085125 USBH_Process gState: 2
085125 USB Device Attached
085625 USBH_Process gState: 5
085625 EnumState : 0
085625 USBH_CtlReq RequestState: 1
085625 USBH_CtlReq RequestState: 2
085625 USBH_HandleControl Control.state : 1
085625 USBH_HandleControl Control.state : 2
089312 USB Device disconnected
089312 USBH_Process gState: 3
089313 USBH_Process gState: 0
091660 USBH_Process gState: 2
091660 USB Device Attached
092160 USBH_Process gState: 5
092160 USBH_CtlReq RequestState: 1
092160 USBH_CtlReq RequestState: 2
092160 USBH_HandleControl Control.state : 1
092160 USBH_HandleControl Control.state : 2
092160 USBH_HandleControl Control.state : 3
092160 USBH_HandleControl Control.state : 4
Any ideas ?
Anyone has USB Host with MSC running on this board ?
best regards
Thomas
2016-11-03 7:26 AM
Hello,
for a new product we want to replace STM32F429 with STM32L476ZGT,
I started to translate our bootloader with USB HOST and MSC class to STM32L476ZGT.
Today our prototype arrived and I got the same problem with enumeratrion as on STM32L476G-DISCO.
any help would be appreciated
best regards
Thomas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.