2023-07-20 10:24 PM
Hello together,
I am currently trying to program a STM32L475RET6. But I have the problem that when I connect the programmer and click on connect, a connection can be established, but it disappears after only a short time with the error "connection lost".
I have already made a few designs and projects with the L4, but never observed such behavior. Has anyone been able to observe this behavior?
Message from STM32Cube Programmer:
06:57:38 : UR connection mode is defined with the HWrst reset mode
06:57:38 : ST-LINK SN : 0036004F3331511934333834
06:57:38 : ST-LINK FW : V3J10M3B5S1
06:57:38 : Board : STLINK-V3SET
06:57:38 : Voltage : 3.29V
06:57:38 : SWD freq : 8000 KHz
06:57:38 : Connect mode: Normal
06:57:38 : Reset mode : Hardware reset
06:57:38 : Device ID : 0x415
06:57:38 : Revision ID : Rev 4
06:57:38 : Debug in Low Power mode enabled.
06:57:38 : UPLOADING OPTION BYTES DATA ...
06:57:38 : Bank : 0x00
06:57:38 : Address : 0x40022020
06:57:38 : Size : 20 Bytes
06:57:38 : Bank : 0x01
06:57:38 : Address : 0x40022044
06:57:38 : Size : 16 Bytes
06:57:38 : UPLOADING ...
06:57:38 : Size : 1024 Bytes
06:57:38 : Address : 0x8000000
06:57:38 : Read progress:
06:57:38 : Data read successfully
06:57:38 : Time elapsed during the read operation is: 00:00:00.002
06:57:40 : Error: Unable to get core ID
06:57:40 : Error: Unable to get core ID
06:57:40 : Error: Unable to get core ID
06:57:40 : Warning: Connection to device 0x415 is lost
06:57:40 : Disconnected from device.
Solved! Go to Solution.
2023-07-22 12:22 AM
I think I have it now, and it's pretty stupid.
Out of desperation I changed the programmer or used a ST-Link V2 from a Nucleo board. First only with the most necessary pins, VCC, SWCLK, SWDIO, NRST and GND.
With this configuration I could suddenly program and debug.
Next I connected the USART pins for the debug outputs and it didn't work anymore.
Then I swapped the USART pins and it suddenly worked again.
So I took the ST-Link V3 again, swapped the pins on the MCU by firmware and lo and behold, that works too.
That means, I will have to swap the RX/TX lines on my PCB
I have now tested this for an hour and it seems to work.
2023-07-20 10:58 PM
Since I don't know for what I have to look, I measured the voltage on each Pin:
While I measured this pins the programmer (ST-Link V3) was connected
2023-07-20 11:58 PM - edited 2023-07-21 12:01 AM
from my experience this happens if
a. connection is bad (bad contact or long wires)
b. spikes from mains coming in ; if you supply target not from USB (where stlink is also) your connection is prone to catch inductive or capacitive coupled spikes from mains;
i had exactly this behavior here at my PC . "connection lost" every some minutes or an hour.
then plugged in mains -> target supply at the PCs (filtered) master-slave socket strip and cable routed near usb-cable to target; target has mains filter and mains earth also; now debug can run many hours without any problem.(and still 2,5m away from PC , stlinkV3 -target cable about 20cm long, at full speed 24MHz + 16Mhz SWO)
try this.
2023-07-21 7:08 AM
Thank you very much for your answer.
I have now done the following to solve the problem:
1. i had to change the 100nF capacitor on the NRST pin of the MCU, was not a short circuit, but had a low impedance, or always a low voltage.
2. noticed that there was no clean 5V coming from the PCB (small dips were noticeable). The PCB was connected via USB-C to a USB-C port on the PC. I have now taken a 5V USB power supply.
With these changes it now looks like it is running stable.
2023-07-21 7:41 AM - edited 2023-07-21 7:42 AM
OK again too early, after 4x code upload I have now again the same problem...
16:35:04 : STM32CubeProgrammer API v2.13.0 | Windows-64Bits
16:35:08 : UR connection mode is defined with the HWrst reset mode
16:35:08 : ST-LINK SN : 0036004F3331511934333834
16:35:08 : ST-LINK FW : V3J11M3B5S1
16:35:08 : Board : STLINK-V3SET
16:35:08 : Voltage : 3.30V
16:35:08 : SWD freq : 8000 KHz
16:35:08 : Connect mode: Normal
16:35:08 : Reset mode : Hardware reset
16:35:08 : Device ID : 0x415
16:35:08 : Revision ID : Rev 4
16:35:08 : Debug in Low Power mode enabled.
16:35:08 : UPLOADING OPTION BYTES DATA ...
16:35:08 : Bank : 0x00
16:35:08 : Address : 0x40022020
16:35:08 : Size : 20 Bytes
16:35:08 : Bank : 0x01
16:35:08 : Address : 0x40022044
16:35:08 : Size : 16 Bytes
16:35:08 : UPLOADING ...
16:35:08 : Size : 1024 Bytes
16:35:08 : Address : 0x8000000
16:35:08 : Read progress:
16:35:08 : Data read successfully
16:35:08 : Time elapsed during the read operation is: 00:00:00.003
16:35:11 : Error: Unable to get core ID
16:35:12 : Error: Unable to get core ID
16:35:12 : Error: Unable to get core ID
16:35:12 : Warning: Connection to device 0x415 is lost
16:35:12 : Disconnected from device.
And now just when I tried it again in the CubeIDE it worked. But I guess as soon as I write this it will not work again.
2023-07-21 8:21 AM
did you plug in the supply on same socket as the PC? + supply should have mains earth (2 pole mini warts may be not so good)
2023-07-22 12:15 AM
Yes it's on the same rail
2023-07-22 12:22 AM
I think I have it now, and it's pretty stupid.
Out of desperation I changed the programmer or used a ST-Link V2 from a Nucleo board. First only with the most necessary pins, VCC, SWCLK, SWDIO, NRST and GND.
With this configuration I could suddenly program and debug.
Next I connected the USART pins for the debug outputs and it didn't work anymore.
Then I swapped the USART pins and it suddenly worked again.
So I took the ST-Link V3 again, swapped the pins on the MCU by firmware and lo and behold, that works too.
That means, I will have to swap the RX/TX lines on my PCB
I have now tested this for an hour and it seems to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.