2018-03-05 4:31 AM
Hi,
i want to send only 1 Pulse and i thought to use a timer.
I use the Board B-L475 iot and i want to generate the pulse on TIM2_ch3 (PA2).
I had build the HAL with stm32cubemx.
Before the while(1) begin i have inserted the following Code:
HAL_StatusTypeDef ret=HAL_TIM_OC_Start(&htim2, TIM_CHANNEL_3);�?�?�?
but when i debug TIM2->are every time 0.
What had i do wrong???
Best Regards...
I have the following config:
#timers #stm32l4-halWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.