2019-09-12 7:51 AM
Hi Guys,
I'm currently using an STM32L452 device and i'm having some problems with the SDIO when using it with DMA.
I have configured DMA and SDIO usign the file generated from STM32Cube tool.
When I try to read the SD card without using DMA , everything works fine.
With the DMA I keep having the RX_OVERRUN error that basically aborts all the DMA interrupts events and then the function remain stucked .
I have searched everywhere for a solution and tryed to apply all of them but i still have the same issue.
Do you know if this is a well known problem and if there is a solution ?
2019-09-12 8:43 AM
I think it is generally accepted that the CubeMX SDIO/SDMMC code output has issues, the forum is full of complaints.
Is this a NUCLEO board, or something custom? For custom report pins used for UART output, HSE clock frequency, etc.
Pretty sure I've had DMA working across all L4/L4+ parts.
2019-09-12 9:02 AM
Hi Clive,
After few attempts I figured out that the DMA works if I enable just one of them ...for example I tried enabling it for RX without configuring the DMA channel for TX...and i can receive the data correctly.
If i try to enable both of them (TX and RX) i have the Overrun issue...
i would like to manage both operations with DMA sincerly..
2019-09-12 9:55 AM
It only ever does one direction at a time. Check how the HAL callbacks are being dispatched. Review HAL example codes for the DISCO/EVAL boards, these tend to have been tested better.
2020-12-09 5:29 AM
hey Guys,
Need your help. I am also facing the same problem. Please Help me.
2020-12-09 5:50 AM
Help you how? You've provided no information about your specific situation, and I doubt you have the same custom board.
The SDIO/SDMMC peripheral, or more specifically the cards, have zero tolerance for you wandering off mid task. Are you using an RTOS?
#MeToo
2020-12-09 7:46 AM
Cross linking these
2020-12-14 11:59 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.