2025-12-17 6:26 AM - last edited on 2025-12-17 7:27 AM by Peter BENSCH
Hello,
I am experiencing the following issue with the STM32L433RCT microcontroller I am using: when I pull the NRST pin LOW and then release it to HIGH, the microcontroller does not recover from reset. In this case, power cycling the device does not solve the problem either. However, if I disconnect the battery from the circuit and then reapply power, the device starts up normally.
This issue occurs mostly during the first boot. After the initial startup is successful, even if I reconnect the battery and pull NRST LOW again, the system does not lock up. I am concerned about what would happen in the field if the device were to freeze and could not recover using a reset.
2025-12-17 7:28 AM - edited 2025-12-17 7:29 AM
That chip boots up into the bootloader when flash is empty. Could be what is happening. You will need to do a power cycle after programming the chip to reset the "flash empty" flag. Just toggling NRST will not do it.
Could also be any number of other issues. Is BOOT0 held low or set via option bytes?
Attach a debugger to see where the chip is at and why it's not functioning correctly.
2025-12-17 10:57 PM
Hello,
I have a piece of code where I only toggle an LED inside the main loop. When I connect the debugger and start the code, everything seems to work normally. However, when the debugger is connected and I power the device off and on again, I notice that the LEDs no longer blink. When I check the NRST and BOOT0 pins, I see that NRST = HIGH and BOOT0 = LOW. When I stop the code, it appears to be stuck at a certain point. You can see the point where it gets stuck in the content named “ek1”, and my user configurations are in the other file.
2025-12-18 12:38 AM
2025-12-18 6:11 AM
It looks like the code is in the default handler which means it's in an interrupt that you haven't implemented. What interrupts are enabled in your code?
You can look at VECTACTIVE field in the SCB registers to see which interrupt it's in. Subtract 16 and compare to IRQn_Type.
> When I try to debug the code that I normally work with, I get the errors shown in the image.
Address 0x1FFFxxxx indicates the chip is in the bootloader.
2025-12-18 9:53 PM
What is the reason that the device stays in the bootloader when it is powered off and on?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.