2018-06-22 1:11 PM
The stm32l4 parts can exit standby/shutdown on either a rising or falling edge of a wake up pin ? Are there any timing constraints ? For example, the adxl362 generates 20 usec pulses in some modes. Is this guaranteed to be sufficient ?
Geoffrey
2018-06-22 5:09 PM
It is likely to be any pulse greater than 1uS will work... 1nS may not work. 20nS would probably be your limit.
I believe this type of circuit is only waiting for a clock pulse from the input, there are no other clocks involved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.