2018-03-01 3:31 AM
Hi
How can we use USART as UART port in STM32L431VCT6 micro controller
I am looking for connecting two STM32L4 micro controller with TX, RX and Ground lines.
Already UART port is being used for other purpose and have only USART port
regards
subramani
#stm32l431vct6-usart-as-uart-port-configurationSolved! Go to Solution.
2018-03-03 4:48 AM
If you could share some thoughts what makes you use USART instead of SPI.
Well, that's simple - all the SPIs are used for other purposes... ;)
JW
2018-03-03 6:45 AM
Exactly, and it's not even a good implementation of synchronous serial, which would minimally have two independent clocks. And lacks any SDLC/HDLC support.
I'm sure the peripheral could be used for other assorted SERDES type implementations, along with SPI, but still a bit of a hack.
2018-03-03 4:30 PM
https://community.st.com/community/stm32-community/blog/2018/03/03/using-usart-instead-of-spi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.