2023-04-25 12:36 AM
uint32_t write_to_flash(uint8_t * buf, uint16_t length){
if((length)>2047) return 0xFFFFFFFF;
uint32_t base_addr=0;
base_addr=getHexAddressPage(DATA_PAGE);
uint32_t PAGEError;
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_PROGERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR |
FLASH_FLAG_SIZERR | FLASH_FLAG_PGSERR | FLASH_FLAG_MISERR | FLASH_FLAG_FASTERR | FLASH_FLAG_OPTVERR);
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
/* Erase the user Flash area*/
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase= FLASH_TYPEERASE_PAGES;
EraseInitStruct.Page = DATA_PAGE;
EraseInitStruct.NbPages= 1;
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
{
DBGx("Flash Erase Fail\r\n");
HAL_FLASH_Lock();
return HAL_FLASH_GetError();
}
for (uint32_t i = 0; i < length; i += 8)
{
uint64_t data64 = u8touint64(buf+i);
PAGEError=HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, i + base_addr, data64);
if (PAGEError != HAL_OK)
{
HAL_FLASH_Lock();
DBGx("2 IS_FLASH_PAGE(Page):%d at mem:%x,PAGEError:%x\r\n",IS_FLASH_PAGE(DATA_PAGE),DATA_PAGE,PAGEError);
return PAGEError;
}
}
HAL_FLASH_Lock();
DBGx("Flash Error:%d\r\n",PAGEError);
return PAGEError;
}Above code is used to write flash
2023-04-25 9:07 AM
Which line return error?
2023-04-25 10:14 PM
At line 20, Flash Erase Fail.
2023-04-26 12:59 AM
Hello @DBhut.1 ,
Could you please check the BankNumber, FirstPage, and NbOfPages.
For that, I recommend you to get inspired from the available FLASH_EraseProgram example in STM32CubeL4 package.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-26 3:05 AM
There is no page issue, as Flash work after first time erase fail, and working fine since 5 months. Only issue is After upload code to fresh MCU, and perform Flash Write, It fails, and we have to perform operation again. So, there may be issue with code or something else, which prevents, Flash to erase, after 1st time only.
2023-04-26 4:24 AM
Hello @DBhut.1 ,
Thank you for this clarification.
Do you have the same issue when you using the ST example?
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-26 4:37 AM
> After upload code to fresh MCU
How do you do that, exactly?
Do you power-down/power-up after finishing code uploading to the mcu?
JW
2023-04-26 5:56 AM
There's another error bit you're not clearing.
Instrument code so you know initial register states and WHY the Erase reportedly fails.
2023-04-26 10:18 PM
I will try thanks
2023-04-26 10:20 PM
No, I don't do any Powerup/down, just flash the code, and write my configuration default values of data to flash, for future use.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.