2025-08-13 5:27 AM
Hi,
I’m working on an STM32L431CBT6 project where I enter STOP2 mode and measure ~1 µA current, which is great. However, I need to use PA0 as a GPIO input to wake up the MCU from STOP2.
When I configure PA0 as an input (no pull, or pull-up/down), my STOP2 current jumps to about 50 µA.
Here’s the relevant setup:
MCU: STM32L431CBT6
Toolchain: CubeMX + HAL
STOP2 entry via HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI)
All unused GPIOs are set to analog mode
PA0 configured as GPIO_MODE_INPUT
Supply voltage: 3.3V
Current measured with multimeter
void Enter_Stop2_Mode(void)
{
// Set all GPIOs to analog
GPIO_InitTypeDef gpio = {0};
gpio.Mode = GPIO_MODE_ANALOG;
gpio.Pull = GPIO_NOPULL;
gpio.Pin = GPIO_PIN_All;
// Set all pins to analog mode
HAL_GPIO_Init(GPIOA, &gpio);
HAL_GPIO_Init(GPIOB, &gpio);
HAL_GPIO_Init(GPIOC, &gpio);
HAL_GPIO_Init(GPIOD, &gpio);
HAL_GPIO_Init(GPIOE, &gpio);
HAL_GPIO_Init(GPIOH, &gpio);
gpio.Pin = V1_Pin;
gpio.Mode = GPIO_MODE_INPUT;
gpio.Pull = GPIO_PULLUP; // or GPIO_PULLDOWN
gpio.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &gpio);
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
printf("entering stop mode\r\n");
Enter_Stop2_Mode();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Question:
Is this higher current expected when keeping a GPIO input active in STOP2? My power budget is around 10uA.
2025-08-20 8:13 AM - edited 2025-08-20 8:24 AM
Hi @ts00882014,
To reduce power consumption in STOP2 mode, you need to configure the unused I/O pins as analog.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.