2016-03-23 1:58 AM
stm32l4xx_hal_spi.h
HAL_SPI_StateTypeDef State; /* SPI communication state */ uint32_t ErrorCode; /* SPI Error code */ stm32l4xx_hal_uart.h __IO HAL_UART_StateTypeDef State; /*!< UART communication state */ __IO uint32_t ErrorCode; /*!< UART Error code */ Why it is __IO in UART and not in SPI ?2016-03-25 7:04 AM
Hi Noyb,
Your question is noted to investigate the reason behind the missing ''__IO'' for SPI.I will keep you informed if I get more details.However I would like to know if you faced any particular issue that leads you to make the update by your self? Or it is just a comment based on code comparison?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-03-29 12:40 AM
Hi Mayla,
the reasons are a little bit from both : 1- issue with the SPI I encountered here : https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32%20SPI%20DMA%20FIFO%20not%20writing%20into%20or%20corrupting%20memory 2- while coding a little serial port framework above HAL, I read the library code to understand how the DMA synchronization was performed on SPI and USART, which lead me to compare structure definitions and find the divergence2016-06-29 5:53 AM
HiNoyb,
Sorry for this delayed update. I checked in the last version of STM32CubeL4 (V1.5.0), we have the following:__IO HAL_SPI_StateTypeDef State;
/*!< SPI communication state */
__IO uint32_t ErrorCode;
/*!< SPI Error code */
-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.