2018-07-02 10:13 AM
Hi,
I am working with an STM32L4. I'm trying to put it into STANDBY mode, and wake it up using a WKUP pin. The issue is that the first time I go to standby after POR, the system wakes up immediately, though I'm sure none of the wakeup pins have had an edge transition. If I go back to STANDBY after that, the system stays in STANDBY. Can anyone explain this behavior? For what it's worth, I am not using a watchdog, I'm turning off the GPIO clocks before going to STANDBY, and I am clearing the standby and WUF flags on every reset. I am including my code for clearing the flags and going to STANDBY.
Thanks,
Ricardo
/* Code for clearing flags, run on every reset */
void SystemStartup(void) {
uint8_t reason = 0; /* Check if the system was resumed from Standby mode */ if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) { /* Clear Standby flag */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); reason |= 0x80; }/* Check and Clear the Wakeup flag */
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF1) != RESET) { __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF1); reason |= 0x01; } if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF2) != RESET) { __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2); reason |= 0x02; } if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF3) != RESET) { __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF3); reason |= 0x04; } if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF5) != RESET) { __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF5); reason |= 0x80; }}/* code for going to STANDBY mode */
void PowerManager::EnterSleepState(void) {
// Wakeup when Qi Charger stops charging - Note CHG♯ is active low HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_HIGH); // Wakeup when device is latched HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_HIGH); // Wakeup when a BLE packet is received HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN3_HIGH); // Wakeup when the user taps the device (accelerometer interrupt) HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN5_HIGH); sysSerial.Print('Going down\r\n'); // Disable GPIO clocks __HAL_RCC_GPIOA_CLK_DISABLE(); __HAL_RCC_GPIOB_CLK_DISABLE(); __HAL_RCC_GPIOC_CLK_DISABLE(); __HAL_RCC_GPIOD_CLK_DISABLE(); __HAL_RCC_GPIOE_CLK_DISABLE(); __HAL_RCC_GPIOF_CLK_DISABLE(); __HAL_RCC_GPIOG_CLK_DISABLE(); __HAL_RCC_GPIOH_CLK_DISABLE(); __HAL_RCC_GPIOI_CLK_DISABLE(); // Enter STANDBY mode - HAL_PWR_EnterSTANDBYMode(); // The rest of this function should never be executed, as the MCU will reset upon wakeup __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOI_CLK_ENABLE(); sysSerial.Print('Getting up\r\n'); // reconfigure the system clock SystemClock_Config(); // reenable I/OHAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1_HIGH);
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN2_HIGH);
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN3_HIGH);
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN5_HIGH);
}
#standby-mode2018-09-18 1:11 AM
Hi,
This is a guesswork, internal wakeup?
Did you checked WUFI bit in PWR_SR1 register?
If it was set, try to clear EIWUL bit (in PWR_CR3).
To do it via HAL, call HAL_PWREx_DisableInternalWakeUpLine() .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.