2019-04-30 6:23 AM
Hi,
is it possible to use the L4's LSE in bypass mode, driven by a 1Hz signal?
I have a set of L4 chips on a bus and would like to feed them a 1Hz / PPS signal from a precise / temperature-compensated clock (and then use the LSE with /1 prescaler for the STM's internal RTC), so their system time is synchronized.
Any reason why this should not work?
At least there seems no minimum frequency for fLSE_ext according to L4 datasheet.
2019-04-30 7:47 AM
>>Any reason why this should not work?
The manual doesn't flag an reasons it shouldn't, PREDIV_S = PREDIV_A = 0 seems valid value, and it talks about division from 1 to 2^22
Suggest you try it. Tend to experiment here when we are "unsure" of how a circuit is implemented or behaves at the corners.
2019-04-30 8:11 AM
Yeah, I got a bunch of nucleos lying around anyway, so I guess I'll just give it a try.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.