2019-01-21 8:10 AM
Hello,
I would like to freeze the functionality of the IWDG while the microcontroller is in STOP mode, because I want stop time greater than 32 seconds. I read the documentation and I built the following code:
FLASH_OBProgramInitTypeDef pOBInit;
pOBInit.OptionType = OPTIONBYTE_USER; // Option byte to be configured
pOBInit.USERType = OB_USER_IWDG_STOP; // User option byte(s) to be configured
pOBInit.USERConfig = OB_IWDG_STOP_FREEZE; // Value of the user option byte
HAL_FLASH_OB_Unlock(); // Unlock the FLASH Option Bytes Registers access.
HAL_FLASHEx_OBProgram(&pOBInit); // Program Option bytes.
HAL_FLASH_OB_Launch(); // Launch the option byte loading.
HAL_FLASH_OB_Lock(); // Lock the FLASH Option Bytes Registers access.But I get a HardFault when executing the unlock function.
Could someone help me with this problem?
Best regards,
2019-01-21 8:22 AM
Hello,
In STOP mode, once the watchdog is enabled, then it cannot be disabled again except by a reset. According to the reference manual: "the IWDG is started by writing to its Key register or by hardware option. Once started it cannot be stopped except by a Reset."
For more details, see Section IWDG functional description in the reference manual.
Kind Regards,
Imen
2019-01-21 8:45 AM
Hello,
I don't want to disable the watchdog, I want to freeze during the STOP mode. In the reference manual section 32.3.4 "Depending on the IWDG_STOP and IWDG_STBY options configuration, the IWDG can
continue counting or not during the Stop mode and the Standby mode respectively.". Then if you go to
the Flash option register (FLASH_OPTR) the Bit 17 (IWDG_STOP) has this definition: Independent watchdog counter freeze in Stop mode.
In order to write this register it is needed to unlock it before, then you write de new value and launch the values writing in OBL_LAUNCH bit in FLASH_CR register.
But something is going wrong and it doesn't work.
2019-01-21 8:45 AM
Dupe
2019-01-21 8:45 AM
Dupe
2019-01-23 5:01 AM
Hello,
I found the solution to my problem, I forgot first to call the function "HAL_FLASH_Unlock ()" to Unlock the FLASH control register access.
But now I have another problem, if I execute the code the microcontroller does not stop resetting again and again. So if I comment the code the options remain saved and the IWDG freezes in STOP mode.
Does anyone know how to avoid this problem?
2019-03-28 4:14 AM
Hello,
It seems that you need to add the following two.
(1) Clear the FLASH's pending flags.
(2) Get the Option bytes configuration, then change pOBInit.
It looks like the following code.
FLASH_OBProgramInitTypeDef pOBInit;
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR); // Clear the FLASH's pending flags.
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBGetConfig(&pOBInit); // Get the Option bytes configuration.
pOBInit.OptionType = OPTIONBYTE_USER;
pOBInit.USERType = OB_USER_IWDG_STOP;
pOBInit.USERConfig = OB_IWDG_STOP_FREEZE;
HAL_FLASHEx_OBProgram(&pOBInit);
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.