2017-05-08 12:11 PM
I'm currently trying to compile the STM32L1xx Discovery Board Example Project with the Dispaly driving, current meassurement and Touch Bar sensing.
I tried to import the Project in TrueSTUDIO on Windows and Linux. Both doesn't work. on Linux I get the following Error on compiling:
20:54:30 **** Rebuild of configuration Debug for project STM32L152RB(STM32L-Discovery) ****
Info: Internal Builder is used for buildarm-atollic-eabi-gcc -c -mthumb -mcpu=cortex-m3 -std=gnu11 -DUSE_STDPERIPH_DRIVER -DSTM32L1XX_MD -I..\..\..\ -I..\..\..\inc -I..\..\..\..\..\Libraries\CMSIS\Include -I..\..\..\..\..\Libraries\CMSIS\Device\ST\STM32L1xx\Include -I..\..\..\..\..\Libraries\STM32L1xx_StdPeriph_Driver\inc -I..\..\..\..\..\Utilities\STM32L-DISCOVERY -Os -ffunction-sections -fdata-sections -g -fstack-usage -Wall -mlong-calls -Wno-pointer-sign -Wno-missing-braces -Wformat=0 -o StdPeriph_Driver/stm32l1xx_syscfg.o ../../../../../Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_syscfg.c ../../../../../Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_syscfg.c:70:30: fatal error: stm32l1xx_syscfg.h: No such file or directory #include 'stm32l1xx_syscfg.h' ^compilation terminated.20:54:30 Build Finished (took 71ms)How can I compile the Project? My favourite method would be a 'universal' Makefile. But ST doesn't provide a Makefile?
2017-05-10 5:47 AM
Hi
kilobyte.ch
,You have to c
heck your configuration project and
make sure that your project has the right include paths and source files from the same tree.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.