2015-05-03 7:46 AM
Hello,
I'm working on custom board using STM32L152 chip. Vref is : 3.19V When i injuct to the analog pin 2.7 i read 4019 ,while 0 represent as 650. (It seemed like 650 is the gap ????) below my initialize ADC code ://///////////////////////////////////////////
RCC_HSICmd(ENABLE);RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
// Configuration CURRENT_SNS pins //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ a_opAdcControl->m_oAdcGpioControl.GPIO_Pin = GPIO_Pin_1; a_opAdcControl->m_oAdcGpioControl.GPIO_Mode = GPIO_Mode_AN; GPIO_Init(GPIOC, &a_opAdcControl->m_oAdcGpioControl); // Configuration Battary test //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ // RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); // a_opAdcControl->m_oAdcGpioControl.GPIO_Pin = GPIO_Pin_4; // a_opAdcControl->m_oAdcGpioControl.GPIO_Mode = GPIO_Mode_AN; // GPIO_Init(GPIOA, &a_opAdcControl->m_oAdcGpioControl);// Check that HSI oscillator is ready while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET);
// ADC1 Configuration ------------------------------------------------------
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); // ADC1 DeInit ADC_DeInit(ADC1); // ADC1 Configuration a_opAdcControl->m_oAdcInitControl.ADC_Resolution = ADC_Resolution_12b; a_opAdcControl->m_oAdcInitControl.ADC_ScanConvMode = DISABLE;// Disable multichannels a_opAdcControl->m_oAdcInitControl.ADC_ContinuousConvMode = DISABLE;// One Conversion at a time a_opAdcControl->m_oAdcInitControl.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;//ADC_ExternalTrigConvEdge_Rising;//ADC_ExternalTrigConvEdge_Falling; a_opAdcControl->m_oAdcInitControl.ADC_ExternalTrigConv =0; a_opAdcControl->m_oAdcInitControl.ADC_DataAlign = ADC_DataAlign_Right; a_opAdcControl->m_oAdcInitControl.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &a_opAdcControl->m_oAdcInitControl); // ADC1 Regular Channel Config // Enables the ADC1 Power Down during Delay ADC_PowerDownCmd(ADC1, ADC_PowerDown_Idle_Delay, ENABLE); // Delay until the converted data has been read ADC_DelaySelectionConfig(ADC1, ADC_DelayLength_Freeze);// Enable ADC1
ADC_Cmd(ADC1, ENABLE); // Wait until the ADC1 is ready while(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET) { } ////////////////////////////////////////////////////////////////The code for reading ch : // a_selCH = 0x0B (ch11 --> PC-1) ADC_RegularChannelConfig(ADC1, a_selCH, 1, ADC_SampleTime_4Cycles); ADC_ClearFlag(ADC1,ADC_FLAG_EOC); // Start the conversion ADC_SoftwareStartConv(ADC1); // Wait until conversion completion while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET){} // Get the conversion value if (ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == SET) { g_opAdcControl->m_oAdcChSample = ADC_GetConversionValue(ADC1); } ADC_ClearFlag(ADC1, ADC_FLAG_EOC); //////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Please advise,2015-05-03 8:44 AM
Try it with more that 4 cycles, and on an STM32L1-DISCO or NUCLEO board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.