2019-02-27 8:00 PM
hello!
Recently, I found such a problem: when the MCU works at 32MHz by default, it can enter the low power mode normally. However, in order to reduce the power consumption during operation, when I reduce the system frequency below 4MHz, the MCU can't enter the low power mode. However, when the system is running above 6MHz, it can enter the low power mode normally. Has anyone tried to sleep normally below 4MHz?
In addition, the MCU is powered by 2.5V.
2019-03-05 1:57 AM
Hello,
Best Regards,
Mohamed Aymen.
2019-06-18 6:30 PM
Hi
@Mohamed Aymen HZAMI
1.I tried HSI�?MSI�?PLL clock source,but they still have the same result.
2.Below is the code that set the system clock to 2MHz.
void SystemClockConfig(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL3;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLL_DIV3;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
assert_param(FAIL);
}
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV8;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
assert_param(FAIL);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
assert_param(FAIL);
}
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq() / 1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
// SysTick_IRQn interrupt configuration
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}3.Below is the code for the MCU to enter and exit stop mode.
void enterStopMode(void)
{
CRITICAL_SECTION_BEGIN();
BoardDeInitMcu();
// Disable the Power Voltage Detector
HAL_PWR_DisablePVD();
// Clear wake up flag
SET_BIT(PWR->CR, PWR_CR_CWUF);
// Enable Ultra low power mode
HAL_PWREx_EnableUltraLowPower();
// Enable the fast wake up from Ultra low power mode
HAL_PWREx_EnableFastWakeUp();
CRITICAL_SECTION_END();
// Enter Stop Mode
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
}
void exitStopMode(void)
{
// Disable IRQ while the MCU is not running on HSI
CRITICAL_SECTION_BEGIN();
// Initilizes the peripherals
BoardInitMcu();
CRITICAL_SECTION_END();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.