2013-07-10 12:51 AM
Hi,
I want to try to send stm32l1 in stop mode (in my experiment I want it never wakes up). My code works but the current is notequal
to datasheet!! In the datasheet the uC in stop mode is around ~2uA In my experiment I have ~15uA!! This my code:int main()
{ SystemInit(); SystemCoreClockUpdate(); PWR_VoltageScalingConfig(PWR_VoltageScaling_Range3); while (PWR_GetFlagStatus(PWR_FLAG_VOS) != RESET) ; RTC_ITConfig(RTC_IT_WUT, DISABLE); LCD_Cmd(DISABLE); while (LCD_GetFlagStatus(LCD_FLAG_ENS) == SET); //******************************************** GPIO IN LOW MODE ******************************************** GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOH,ENABLE); /* Configure all GPIO port pins in Analog input mode (trigger OFF) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_400KHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIOA->MODER = 0xFFFFFFFF; GPIOB->MODER = 0xFFFFFFFF; GPIOC->MODER = 0xFFFFFFFF; GPIOD->MODER = 0xFFFFFFFF; GPIOE->MODER = 0xFFFFFFFF; GPIOH->MODER = 0xFFFFFFFF; /* all GPIOA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_Init(GPIOA, &GPIO_InitStructure); /* All GPIOC except PC13 which is used for mesurement */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_Init(GPIOC, &GPIO_InitStructure); /* all GPIOB except PB6 and PB7 used for LED*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All ; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All ; GPIO_Init(GPIOD, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All ;
GPIO_Init(GPIOH, &GPIO_InitStructure); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,DISABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,DISABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,DISABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD,DISABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOH,DISABLE); PWR_PVDCmd(DISABLE); //******************************************** RUN 4 Mhz in low power ******************************************** PWR_FastWakeUpCmd(DISABLE); SetHSICLKToMSI(RCC_MSIRange_6,NoDIV2,WITHRTC) ; SysTick->CTRL = 0; RCC->APB1ENR = 0; PWR_UltraLowPowerCmd(ENABLE); while(1){ /* Enter Stop Mode permanently !!!!*/ PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI); }2013-07-10 1:28 AM
Hello Michele,
The pins configuration isn't so clean compared to the comments. This config should be enough to put pins in analog input mode:RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOG,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOH,ENABLE);
GPIOA->MODER = 0xFFFFFFFF;
GPIOB->MODER = 0xFFFFFFFF;
GPIOC->MODER = 0xFFFFFFFF;
GPIOD->MODER = 0xFFFFFFFF;
GPIOE->MODER = 0xFFFFFFFF;
GPIOF->MODER = 0xFFFFFFFF;
GPIOG->MODER = 0xFFFFFFFF;
GPIOH->MODER = 0xFFFFFFFF;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOG,DISABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOH,DISABLE);
I listed all ports and depending on your package you can choose only the available ones.
This is just for check, not sure it is the problem root cause.
-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-07-10 3:02 AM
I have checked,
I have 64pin I have this port:RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOH,ENABLE);
All ports are disable but I have 15uA
instead of
~2uA2013-07-10 4:35 AM
target
reached
! now <2uA !! The code work but the difference are the order of function: before (~15uA): //RUN 4MHZ PWR_FastWakeUpCmd(DISABLE); SetHSICLKToMSI(RCC_MSIRange_6,NoDIV2,WITHRTC) ; SysTick->CTRL = 0; RCC->APB1ENR = 0; PWR_UltraLowPowerCmd(ENABLE); After(<2uA) //RUN 4MHZ PWR_FastWakeUpCmd(DISABLE); PWR_PVDCmd(DISABLE); PWR_UltraLowPowerCmd(ENABLE); RCC->APB1ENR = 0; SysTick->CTRL = 0; SetHSICLKToMSI(RCC_MSIRange_6,NoDIV2,WITHRTC) ;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.