cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 bricked after attempting USB

matthewjames32
Associate
Posted on August 14, 2014 at 14:13

I have about 5 different projects using STM32 F series and 2 using STM32L151 on custom board.   I use the ST-link V2 to program and debug them.

I was attempting to get a custom board with USB port working.  I loaded in custom code that setup the clocks and USB with some of the modified virtual com port examples and my own code to toggle the LEDS etc on the board.  After running the code ( initially with the wrong clock speed which I could reset using the BOOT pins to boot into system memory) . 

My board no longer connects via the st-link utility.  St link is fine as talks to other projects fine.  I have had the same thing happen on 2 boards.

Re-powering doesn't fix it. I can't boot into system memory to get out of it.   My code (that flashes LEDS etc still runs if I re-power.

Is there any way the USB bootloader is permanently active?

Any other suggestions as to how to reset the boards to give me control or have I somehow bricked them.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 14, 2014 at 14:24

ST-LINK Utilities, go to Target->Settings properties and select ''Connect under Reset'', reset the chip with BOOT0 pulled High.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.