2025-10-06 3:33 AM
Heyho,
just checking the L162 for a new project, then found that the ADC can only be clocked by the HSI.
Is that correct?
If yes, why?
My experience with HSI (and other RC-oscillators) is that it is "mediocre" at best, rather inaccurate and jitters like crazy. Although this might not be a big issue with a 12-bit ADC.
Merci!
Solved! Go to Solution.
2025-10-06 5:31 AM
Hello @LCE
I confirm that the ADC is clocked only by HSI. For the reason behind this design choice, according to the chapter 12.3.2 of the RM0038:
"To avoid unnecessary consumption while not converting, the ADC digital interface has been designed to operate in a completely independent manner, at its maximum speed using an internal 16 MHz clock source (HSI), whatever the CPU operating frequency (which can range from a few sub-kHz up to 32 MHz)."
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-06 5:31 AM
Hello @LCE
I confirm that the ADC is clocked only by HSI. For the reason behind this design choice, according to the chapter 12.3.2 of the RM0038:
"To avoid unnecessary consumption while not converting, the ADC digital interface has been designed to operate in a completely independent manner, at its maximum speed using an internal 16 MHz clock source (HSI), whatever the CPU operating frequency (which can range from a few sub-kHz up to 32 MHz)."
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-06 6:27 AM
Thanks for the info.
Bad idea anyway. ;)
But probably no game stopper for my application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.