2018-03-15 4:13 AM
I'm drawing a new design with the STM32L071KBUx #UFQFPN32.
Do I have to connect the exposed pad to the GND, or can I leave it open. I don't see any note in the datasheet DM00141136.pdf, so I think that I can leave it open ?
2018-03-15 3:58 PM
connected to ground usually, can you use a meter to check it ?
the smaller QFN style chip has the rating like 36degrees raise in temp at 1W...
these stm32L parts are supposed to be low power,
at 32MHz I cant see then getting warm.
do you have one running ?, does it get hot ?
2018-03-16 12:40 AM
I don't have the device yet (proto phase).
2018-03-16 1:04 AM
It’s not mentioned in the data sheet, so don’t connect it.
I would be surprised if the chip gets warm under load,
You would have to make that assessment when you have it running.
Otherwise on the PCB, just send a couple of via’s through and heat sink it.. a bit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.