cancel
Showing results for 
Search instead for 
Did you mean: 

Package UFQFPN32 (5x5 mm) for STM32F302x6 STM32F302x8

ATrem.1
Associate II

Hi,

The package UFQFPN32 (5x5 mm) have an exposed pad but where is the definition of this Exposed Pad in the datasheet for the STM32F302K8 K Must I connect to the GND or is it not connected or maybe another pin definition ? I can't see in the datasheet.

Thanks for your help.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hello @ATrem.1​  and @Community member​ ,

Indeed the note to be added is the following: "“There is an exposed die pad on the underside of the UFQFPN package. It is recommended to connect and solder this back-side pad to PCB ground".

We need to wait for new document release to add it.

Thanks,

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

9 REPLIES 9
waclawek.jan
Super User

This is a recurring question, see e.g. https://community.st.com/s/question/0D50X00009XkZOtSAN/stm32f301k8u6-connection-of-exposed-pad , https://community.st.com/s/question/0D50X00009XkWZWSA3/stm32f301kxux-exposed-pad-of-ufqfpn-package-connection , https://community.st.com/s/question/0D50X00009XkX5mSAF/stm32l071kbux-ufqfpn32-exposed-pad .

I can't find the mentioned remark in DocID025147 rev.7 (STM32F302x6 STM32F302x8 DS) nor in DS9895 Rev 8 (STM32F301x6 STM32F301x8).

@Amel NASRI​  , could this please be resolved, possibly for all the relevant DS with packages which have exposed pad?

JW

Amel NASRI
ST Employee

Hello @ATrem.1​  and @Community member​ ,

Indeed the note to be added is the following: "“There is an exposed die pad on the underside of the UFQFPN package. It is recommended to connect and solder this back-side pad to PCB ground".

We need to wait for new document release to add it.

Thanks,

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

waclawek.jan
Super User

Thanks, Amel.

JW

ATrem.1
Associate II

Thanks, Amel.

So it's the same for a lot of STM32 references with the same package. The STM32L432KC is in this case ?

Need to check for STM32L432KC.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

ATrem.1
Associate II

For my board, I connected it to the GND and it's working. I hope no problem later...

Amel NASRI
ST Employee

Note added for F302 datasheet (https://www.st.com/resource/en/datasheet/stm32f302r6.pdf).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, Amel.

JW

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.