2018-08-02 10:21 PM
I'm trying to stop the processor for 9s and run for 1s using the low power timer. All my attempts have failed and I can't get it to work. Once its running it needs to switch ON the LED, transmit a packet and wait for few seconds for commands from a LoRa radio module. Before it goes to stop mode it needs to switch OFF the LED. I'm using STM32 systemworkbench and CubeMX for development. I would appreciate if someone could give me any help with this.
LPTIM is configured as follows:
Clock source: LSI
Prescaler: DIV16
Update Mode: Immediate
Trigger Source: Software Trigger
Timeout Period = 9s
Compare = (Timeout period*LSI_Frequency/Prescaler )-1
= 20,812
Period = 41,634
Below I have attached a sketch of the code.
void HAL_LPTIM_CompareMatchCallback(LPTIM_HandleTypeDef *hlptim)
{
/* Timeout was reached */
Sleep_Timeout = 1;
}void Sleep(){
//Switch off PWM to turn off LED
if(!run_once){
if (HAL_LPTIM_TimeOut_Start_IT(&hlptim1, LPTIM_Period, LPTIM_Timeout) != HAL_OK)
{
Error_Handler();
}
run_once = 1
//Transmit sleep message
}
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* ### - 4 - Enter in Stop mode ########################################### */
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
if(Sleep_Timeout) {
//Switch ON LED
//Transmit sleep message
//Wait 1s for incoming commands
Sleep_Timout = 0
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.