2016-09-07 10:28 AM
Hi there! I'm using the STM32L053 Discovery board, and I'm having a very weird problem. Whenever I remove power from the board, whatever is in the first page of flash disappears. The first 3 words become random (changes every power cycle) and everything else is erased to 0. Since this is the vector table spot, my image doesn't run after I remove power and I have to reprogram it.
I was originally using Visual Studios with VisualGDB, but I just got the OpenSTM32 workbench thingie running and did two of the examples from the L0 framework and programmed the resulting images using the ST-LINK Utility. Exact same result.What am I missing? Why does the first page of flash keep getting reset? Any help would be greatly appreciated.Thanks!Edit: Forgot to mention, this occurs on two separate Discovery boards and I believe it happened out of the box. I haven't changed any protection levels or anything like that but I did confirm that they are all off. #flash #stm32l0 #vectortabl2016-09-07 11:46 AM
Not something I've heard described here before, are you sure it's not your debugger doing this?
The ST-LINK mbed firmware? Make sure you have current ST-LINK firmware via the v3.9.0 Utilities.2016-09-07 12:49 PM
I was afraid it was the debugger, which is why I moved to programming it using the St-Link. Then I was afraid it was the image, so I downloaded the Eclipse based tool and compiled one of the example projects. Then I went and upgraded ST-Link from version 3.7.0 to 3.9.0. Nothing. Nada. Ziltch. I'm so confused. I have an L4 discovery board that works perfectly fine and my company is shipping a product with an L1 in it that I've been working on for over a year and that works fine too.
Fun fact that I just determined. The first page of flash is only erased when I power the L0 unit via the ST-Link port. I have an L4 with SPI and power hooked up to an L0 and I use the memory boot mode to program the L0 via the SPI protocol. Since I can power both just by plugging in at the ST-Link port on the L4, I can power cycle the L0 without touching it's ST-Link port. If I do that, the flash page does not get erased.I also checked power the L0 board using it's USB port instead of it's ST-Link port and that seems to be OK too. Just when I use the ST-Link port... soooo yea. Kinda of annoying but not as horrible as it seemed a few hours ago.Edit: With the new version of ST-Link, I noticed a little bit at the top of the status box when I connected to the L0 board. The ST-Link firmware needed to be updated. I did that and now it's fine.... *facepalm*So... solved I guess. If anyone else has this problem, update the firmware on your L0 boards ST-Link...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.