2016-11-03 9:47 PM
Solved! Go to Solution.
2017-01-13 6:43 AM
Hello
76386
andLabrado.Jeremy
,This issue has been solved and delivered in CubeMX4.
Don't hesitate to upgrade CubeMX release in order to avoid this issue.
Thanks and best regards.
Eric
2016-11-16 2:55 AM
Hichan.herwin,
Please try removing the following code from the ADC2 configuration and let me know please if the problem is resolved then:#if 0
/**Configure the ADC multi-mode
*/
multimode.Mode = ADC_DUALMODE_REGSIMULT;
multimode.DMAAccessMode = ADC_DMAACCESSMODE_12_10_BITS;
multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_1CYCLE;
if
(HAL_ADCEx_MultiModeConfigChannel(&hadc2, &multimode) != HAL_OK)
{
Error_Handler();
}
#endif
-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-01-04 4:56 PM
Hi chan.herwin,
Have you find a way to read the two ADCs simultaneously finally?
I am having the same problem so we can maybe help each other.
Cheers,
Jeremy
2017-01-13 6:43 AM
Hello
76386
andLabrado.Jeremy
,This issue has been solved and delivered in CubeMX4.
Don't hesitate to upgrade CubeMX release in order to avoid this issue.
Thanks and best regards.
Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.