2023-09-06 11:41 AM
Hello all
i have a board with STM32H743BIT6 on it with 4 INTERNAL ADC pin connected to resistor ladders.
i connected external 2.5V reference and defined in the IOC file to use external reference.
i have constant offset of +150mV and all readings of the ADC inputs.
how can i compansate that offset by any type of SW manner, or calibration method?
the ADC is 16 bits and i use the formula:ADC_VALUE[dec]=Vadc*(2^16-1)/2.5.
all the reading ge offset of +3902[dec] +150mV.
2023-09-06 12:18 PM - edited 2023-09-06 12:21 PM
1. what voltage at pin - real ? check with dmm.
2. connect pin to gnd, then test adc...
3. do calibration cycle first ! did you ? offset and linearity ?
4. adc sampling time ...set to 7.5 or so.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.