2021-07-13 4:01 AM
I'm using the 4K of battery backed RAM on the STM32H743 to preserve variables between power cycles. This works fine on 90% of identical systems running identical firmware and with identical H/W, identical chip versions etc. i.e. data is exactly what it should be after power cycling. I always flush the cache after writing to the RAM as this is a known issue.
On a small percentage of systems the Backup RAM is completely overwritten and this is always to the same values. Obviously I've checked the batteries and the RTC keeps time after power cycling so I know the RTC power domain is OK.
I'm at a loss as to where to look for the problem - any ideas appreciated.
The initialisation code for the RAM is taken from the ST example code and as explained above on most versions of "identical" H/W with identical firmware works perfectly.
On all systems the RAM is correct after a reset, it is only after a power cycle that I see the problem
2021-07-13 6:36 AM
How often d you write to battery backed RAM. Maybe do not memory map, but use a function to read/write that memory and only enable the clock while in the function.
2021-07-13 7:04 AM
1. Catch the false write
2. Robust with dual block
Paul
2021-07-13 7:06 AM
3. If available catch "brownout" events or reset on brownout to prevent MCU from running on unreliable power.
2021-07-13 8:15 AM
Thanks for the ideas.
The backup ram is only being written very infrequently and only when the user actions a specific request from the UI. It is only written from a single function. As the backup ram is non-contiguous with other memory then any "rogue" write would likely trigger a bus error. Note also that the write survives a reset perfectly. It is something to do with the power-down/power-up sequence that causes the problem. I'll add a brown-out interrupt to immediately put the processor into reset but am not hopeful this will help
2021-07-13 8:48 AM
Most likely it's a program bug resulting in overwriting the backup RAM.
Is backup-domain write disabled all the time except when writing to the NVRAM/RTC?
Place a data breakpoint ("watchpoint") to the BKPSRAM and observe, what are the sources of writes.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.