2020-06-24 12:53 AM
Hello,
I use STM32H742 rev V. In contrast to rev Y register ADCx->CR has two bits BOOST. I set both, because I want the highest ADC speed. But reading ADCx->CR back, with the debugger or in the running program reports only BOOST 0 set. What is wrong there or did I miss something? ADC seems to run fine at 3.8 Msps.
Any help is welcome
Martin
2020-06-24 7:21 AM
> STM32H742 rev V. ... register ADCx->CR has two bits BOOST.
Where are you seeing this information?
2020-06-29 10:56 PM
Hello TDK,
sorry for the delay...
It is in the reference manual RM0433 rev 6, chapter 24.6.3. holds the description of register ADCx->CR and there are two sections, one for rev Y and one for rev V.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.