2020-05-19 1:39 AM
Hello,
I'm doing some tests on the STM32H743 FPU (on a Nucleo, from Keil v5 IDE).
I've checked that the FPU is enabled (register CPACR) and I've written a basic division by 0 test .
volatile double test = 0;
test = 1.0 / test;I checked the assembly code. I've got as expected the following instruction:
VDIV.F64 d0,d0,d1where d1 contains 0x00...00 (numerical value 0) and d0 contains 0x3FF00...00 (numerical value 1).
The instruction executes but the result (value in d0) remains the same (0x3F00...00) and there is no flag indicating the division by zero exception (flag DZC in FPSCR).
If I do the same test in single precision
volatile float test = 0;
test = 1.0f / test;the result after
VDIV.F32 s0,s2,s0in s0 is indeed a float representation for infinity.
What am I missing ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.