2023-08-30 2:20 AM
Hi,
I could use some help getting started with SPI5 (limited feature set). I want to operate as SPI master and send a single byte. I want to control SS manually as ordinary GPIO out.
I've enabled the peripheral clock, and I can see in the debugger that FIFO flag TXTF goes high when I write to TXDR, and that I set CSTART. But nothing comes on MOSI or SCK, and EOT is never set.
Do you spot anything obvious in the code below?
What puzzles me is that if I set SSIOP = 0 and use the same code, TXTF and CSTART is not set. SSIOP should not be of importance when the peripheral is not in control of SS, right?
// Enable AF on MOSI, MISO, SCK. Set CS 1 and 2 as outputs (manual control).
GPIOF->MODER = (GPIOF->MODER & 0b11111111111100000011110000111111) | 0b00000000000010101000000101000000;
SPI5->CFG1 = 0b01110000000000000000000000000000;
SPI5->CFG2 = 0b10010001010000000000000000000000;
SPI5->CR2 = 1;
SPI5->CR1 = BIT(0);
SPI5->IFCR |= BIT(3); // Clear EOT flag.
SPI5->TXDR = data; // Load FIFO.
SPI5->CR1 |= BIT(9); // Transfer start.
// Wait for EOT.
while ((SPI5->SR & BIT(3)) == 0)
;
Solved! Go to Solution.
2023-09-04 4:09 AM
I solved it.
With the two lines below missing, the MCU got stuck waiting for an EOT that never came.
// Select AF5 (SPI MOSI, MISO and SCK) on PORTF[9:7]
GPIOF->AFR[0] |= 0x50000000;
GPIOF->AFR[1] |= 0x00000055;
I would have expected nothing to show up on the I/O-pins, but not the actual register writing and reading to be affected. Oh well, assumption is the mother of all **bleep** ups :)
Attached is the working code.
2023-09-04 4:09 AM
I solved it.
With the two lines below missing, the MCU got stuck waiting for an EOT that never came.
// Select AF5 (SPI MOSI, MISO and SCK) on PORTF[9:7]
GPIOF->AFR[0] |= 0x50000000;
GPIOF->AFR[1] |= 0x00000055;
I would have expected nothing to show up on the I/O-pins, but not the actual register writing and reading to be affected. Oh well, assumption is the mother of all **bleep** ups :)
Attached is the working code.
2023-09-04 4:10 AM
Good job :flexed_biceps:
Mark your answer as best answer to be diffused to everyone.
Best regards.
II
2024-04-04 11:35 PM
Does your code works fine?
And did you make // TODO: ensure TXP == 1 in SR?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.